Real Time

PDCCH Transmission Configuration (Basic LTE FDD Downlink)

In the Physical Channel node, select a PDCCH channel, then click the button in the Transmission Configuration cell to open the PDCCH Transmission Configuration dialog box. Click the Column Preset button to access a Closeddrop-down list that enables you to set the parameters for all PDCCH transmissions to the same value.

State

Choice: On | Off  

Default: Off

Check (On) or clear (Off) to set the channel state.

Data

Use the Data Source Selection dialog box to select PN9, PN15, or User Defined Bits to use for the data.

CCE Aggregation Level

Use the drop-down list to select a control channel element (CCE) aggregation level of 1, 2, 4, or 8.

CCE Offset

The choices available for control channel element (CCE) offset are determined by the CCE aggregation level as follows:

CCE Aggregation Level

CCE Offset choices

1

0 | 1 | 2 |... N_PDCCHmax -1

2

0 | 2 | 4 |... N_PDCCHmax -1

4

0 | 4 | 8 |... N_PDCCHmax -1

8

0 | 8 | 16 |... N_PDCCHmax -1